Feedback_Position_Error_Limit

Index.Sub  2230.01H
Data Type Unsigned32
Access Read/Write
PDO Mappable No
Unit

IU (one motor turn = 65536 IU)

Range

Unsigned32
Default Value 10000
Store Supported Yes
Description This value is used for Closed Loop feature and defines the maximum allowed displacement between motor reference position and motor actual position detected by Feedback Sensor.

Notes

--